cancel
Showing results for 
Search instead for 
Did you mean: 

Handling of more than 15 EXTI lines

patrickschneider9
Associate III

Hi there,

I just wondered if any of you would have an idea about my current problem, or faced similar challenges:

For a new project I would need about 20 configurable EXTI lines, which exceeds the number of any STM32 MCU as far as we know. How could we still achieve that with additional hardware circuitry or any "tricks" on the MCU? I thought about having DMA configured to read GPIO registers to a memory buffer, but don't know if that will really work.

Any ideas are appreciated!

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12

one chip, TI, 24 inputs. Or 16 inputs.

patrickschneider9
Associate III

I need to be able to detect up to 15kHz PWM and the corresponding duty cycle.

I need to be able to detect up to 15kHz PWM and the corresponding duty cycle.