cancel
Showing results for 
Search instead for 
Did you mean: 

Hall sensors not triggering IRQ from TIMER2

Bogdan
Senior
Posted on January 02, 2017 at 18:14

Hello,

i am working on a bldc motor project for school, and for start to understand whats happening inside the IRQ handler, i have configured timer2  on ch1,2,3 with 3 emulated hardware signals, imitating the CW of a bldc motors

The hall emulated signals are coming from another development board. The signals are bellow

0690X00000605yKQAQ.png

These signals ( H1,H2,H3) are feed into a STM32F407 device, on PA0, PA1 and PA2   which are Ch1,2,3 of the TIMER2 

i have prepared only the initialization of the timer2 to see if the hall signals trigger the CC1 event in the irq handler, but its not triggering.

I've put a small toggle on a PC1 pin just to see when its triggering inside the TIM2_IRQhandler,

But there is no triggering,

At this point Timer1 is not initialized, i just want to see how it behaives on the hall signals.

I am missing something?  Of does the Timer2 takes some kind of feedback from TIM1 in order to trigger CC1 event?

void timer2_setup(void){

GPIO_InitTypeDef GPIO_InitStructure;

RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 |GPIO_Pin_2;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;

GPIO_Init(GPIOA, &GPIO_InitStructure);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_TIM2);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_TIM2);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_TIM2);

//**** PC1 is used for toggle in IRQ handlers to see with logic analyzer

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 ;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;

GPIO_Init(GPIOC, &GPIO_InitStructure);

NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 7;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 7;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

TIM_TimeBaseStructure.TIM_Prescaler = 126;

TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

TIM_TimeBaseStructure.TIM_Period = 65530;

TIM_TimeBaseStructure.TIM_ClockDivision = 0;

TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;

TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

TIM_SelectHallSensor(TIM2, ENABLE);

TIM_SelectInputTrigger(TIM2, TIM_TS_TI1F_ED);

TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Reset);

TIM_SelectMasterSlaveMode(TIM2, TIM_MasterSlaveMode_Enable);

TIM_ICInitStructure.TIM_Channel = TIM_Channel_1 ;

TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_BothEdge;

TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_TRC;// listen to T1, the HallSensorEvent

TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;// Div:1, every edge

TIM_ICInitStructure.TIM_ICFilter = 0;

TIM_ICInit(TIM2, &TIM_ICInitStructure);

// Enable CC1 interrupt request

TIM_ITConfig(TIM2, TIM_IT_CC1, ENABLE);

TIM_Cmd(TIM2, ENABLE);

}

void TIM2_IRQHandler(void){

if (TIM_GetITStatus(TIM2, TIM_IT_CC1) != RESET)

{

GPIO_ToggleBits(GPIOC,GPIO_Pin_1); // Toggle the pin for logic analyzer

TIM_ClearITPendingBit(TIM2, TIM_IT_CC1);

}

}

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on January 26, 2017 at 09:46

Hi

Anton.Bogdan

,

Thanks for sharing the solution.This will be helpful for other users.

Khouloud