2023-02-27 11:49 PM
Hi!
I am trying to write a program where I am waiting for receiving 6 bytes of data through UART. It works just fine the first time, than I restart the receive_IT function and nothing happens anymore. I have other codes where I use it just the same, the only difference is the MCU. For this project I am using an STM32F030F4P6.
main.c
volatile uint8_t rx_buffer[6] = {0};
int8_t step = 1;
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_TIM3_Init();
MX_USART1_UART_Init();
MX_TIM14_Init();
/* USER CODE BEGIN 2 */
HAL_UART_Receive_IT(&huart1, rx_buffer, 6);
HAL_GPIO_WritePin(Sleep_X_GPIO_Port, Sleep_X_Pin, GPIO_PIN_SET);
HAL_GPIO_WritePin(Sleep_Y_GPIO_Port, Sleep_Y_Pin, GPIO_PIN_SET);
HAL_GPIO_WritePin(Sleep_Z_GPIO_Port, Sleep_Z_Pin, GPIO_PIN_SET);
HAL_GPIO_WritePin(Step_X_GPIO_Port, Step_X_Pin, GPIO_PIN_RESET);
HAL_GPIO_WritePin(Step_Y_GPIO_Port, Step_Y_Pin, GPIO_PIN_RESET);
HAL_GPIO_WritePin(Step_Z_GPIO_Port, Step_Z_Pin, GPIO_PIN_RESET);
HAL_GPIO_WritePin(Dir_GPIO_Port, Dir_Pin, GPIO_PIN_RESET);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}stm32f0xx_it.c
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart){
/*
* x, e = 221
* x, h = 224
*
* y, e = 222
* y, h = 225
*
* z, e = 223
* z, h = 226
*
* p, k = 219
* p, b = 210
*/
for(i=0; i<2; i++){
sum_rx += rx_buffer[i];
}
for(i=2;i<6;i++){
sum_step += ((rx_buffer[i] - 48) * power(10, 5-i));
}
/*sum_step += (rx_buffer[5] - 48);
sum_step += ((rx_buffer[4] - 48) * 10);
sum_step += ((rx_buffer[3] - 48) * 100);
sum_step += ((rx_buffer[2] - 48) * 1000);*/
switch(sum_rx){
case 221:
HAL_GPIO_WritePin(Dir_GPIO_Port, Dir_Pin, GPIO_PIN_RESET);
HAL_GPIO_WritePin(Sleep_X_GPIO_Port, Sleep_X_Pin, GPIO_PIN_SET);
for(i=0; i<sum_step; i++){
HAL_GPIO_WritePin(Step_X_GPIO_Port, Step_X_Pin, GPIO_PIN_SET);
Delay(2);
HAL_GPIO_WritePin(Step_X_GPIO_Port, Step_X_Pin, GPIO_PIN_RESET);
}
HAL_GPIO_WritePin(Sleep_X_GPIO_Port, Sleep_X_Pin, GPIO_PIN_RESET);
break;
case 224:
HAL_GPIO_WritePin(Dir_GPIO_Port, Dir_Pin, GPIO_PIN_SET);
HAL_GPIO_WritePin(Sleep_X_GPIO_Port, Sleep_X_Pin, GPIO_PIN_SET);
for(i=0; i<sum_step; i++){
HAL_GPIO_WritePin(Step_X_GPIO_Port, Step_X_Pin, GPIO_PIN_SET);
Delay(2);
HAL_GPIO_WritePin(Step_X_GPIO_Port, Step_X_Pin, GPIO_PIN_RESET);
}
HAL_GPIO_WritePin(Sleep_X_GPIO_Port, Sleep_X_Pin, GPIO_PIN_RESET);
break;
case 222:
HAL_GPIO_WritePin(Dir_GPIO_Port, Dir_Pin, GPIO_PIN_RESET);
HAL_GPIO_WritePin(Sleep_Y_GPIO_Port, Sleep_Y_Pin, GPIO_PIN_SET);
for(i=0; i<sum_step; i++){
HAL_GPIO_WritePin(Step_Y_GPIO_Port, Step_Y_Pin, GPIO_PIN_SET);
Delay(2);
HAL_GPIO_WritePin(Step_Y_GPIO_Port, Step_Y_Pin, GPIO_PIN_RESET);
}
HAL_GPIO_WritePin(Sleep_Y_GPIO_Port, Sleep_Y_Pin, GPIO_PIN_RESET);
break;
case 225:
HAL_GPIO_WritePin(Dir_GPIO_Port, Dir_Pin, GPIO_PIN_SET);
HAL_GPIO_WritePin(Sleep_Y_GPIO_Port, Sleep_Y_Pin, GPIO_PIN_SET);
for(i=0; i<sum_step; i++){
HAL_GPIO_WritePin(Step_Y_GPIO_Port, Step_Y_Pin, GPIO_PIN_SET);
Delay(2);
HAL_GPIO_WritePin(Step_Y_GPIO_Port, Step_Y_Pin, GPIO_PIN_RESET);
}
HAL_GPIO_WritePin(Sleep_Y_GPIO_Port, Sleep_Y_Pin, GPIO_PIN_RESET);
break;
case 223:
HAL_GPIO_WritePin(Dir_GPIO_Port, Dir_Pin, GPIO_PIN_RESET);
HAL_GPIO_WritePin(Sleep_Z_GPIO_Port, Sleep_Z_Pin, GPIO_PIN_SET);
for(i=0; i<sum_step; i++){
HAL_GPIO_WritePin(Step_Z_GPIO_Port, Step_Z_Pin, GPIO_PIN_SET);
Delay(2);
HAL_GPIO_WritePin(Step_Z_GPIO_Port, Step_Z_Pin, GPIO_PIN_RESET);
}
HAL_GPIO_WritePin(Sleep_Z_GPIO_Port, Sleep_Z_Pin, GPIO_PIN_RESET);
break;
case 226:
HAL_GPIO_WritePin(Dir_GPIO_Port, Dir_Pin, GPIO_PIN_SET);
HAL_GPIO_WritePin(Sleep_Z_GPIO_Port, Sleep_Z_Pin, GPIO_PIN_SET);
for(i=0; i<sum_step; i++){
HAL_GPIO_WritePin(Step_Z_GPIO_Port, Step_Z_Pin, GPIO_PIN_SET);
Delay(2);
HAL_GPIO_WritePin(Step_Z_GPIO_Port, Step_Z_Pin, GPIO_PIN_RESET);
}
HAL_GPIO_WritePin(Sleep_Z_GPIO_Port, Sleep_Z_Pin, GPIO_PIN_RESET);
break;
case 219:
htim3.Instance -> CCR1 = ki;
HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_1);
Delay(150);
HAL_TIM_PWM_Stop(&htim3, TIM_CHANNEL_1);
break;
case 210:
htim3.Instance -> CCR1 = be;
HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_1);
Delay(150);
HAL_TIM_PWM_Stop(&htim3, TIM_CHANNEL_1);
break;
default:
break;
}
for(i=0; i<7; i++){
rx_buffer[i] = 0;
}
HAL_UART_Receive_IT(huart, rx_buffer, 6);
step = 1;
sum_rx = 0;
sum_step = 0;
}
void Delay(uint8_t ms){
HAL_TIM_Base_Start(&htim14);
while(htim14.Instance -> CNT < ms){
}
htim14.Instance -> CNT = 0;
HAL_TIM_Base_Stop(&htim14);
}
int power(int x, int y){
int i;
int eredm = x;
if(y != 0){
for(i=1; i<y; i++){
eredm *= x;
}
}
else
eredm = 1;
return eredm;
}I also tried not to call the HAL_UART_Receive_IT() inside the callback function, nothing else happened. I also checked the UART registers and everything seems the same as when I call the function the first time.
Thank you in advance!
********
Edit:
Thank you for the answers but today I was able to find the solution, yet I still don’t know why.
So Inoticed that the EIE bit in CR3 register don’t set to 1 after the second call of the HAL_UART_Receive_IT() function, but if I set it to 1 by hand before the function it works just fine.
Solved! Go to Solution.
2023-03-03 6:43 AM
Thank you for the answers but today I was able to find the solution, yet I still don’t understand.
So Inoticed that the EIE bit in CR3 register don’t set to 1 after the second call of the HAL_UART_Receive_IT() function, but if I set it to 1 by hand before the function it works just fine.
2023-08-15 6:44 AM
Thank you @BBara.1 , I'm running into this same weird issue and calling MX_USART1_UART_Init() worked for allowing more interrupt reads.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.