HAL_I2C_IsDeviceReady problem and others
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-05-03 5:07 AM
Posted on May 03, 2016 at 14:07
It's normal that you send the timeout to this function and inside call I2C_WaitOnFlagUntilTimeout with I2C_TIMEOUT_BUSY_FLAG, ( 10 seconds ) ?
If not ready, this function block all for about 10 seconds indipendently from timeout settedHAL_StatusTypeDef HAL_I2C_IsDeviceReady(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint32_t Trials, uint32_t Timeout){ uint32_t tickstart = 0, tmp1 = 0, tmp2 = 0, tmp3 = 0, I2C_Trials = 1; if(hi2c->State == HAL_I2C_STATE_READY) { /* Wait until BUSY flag is reset */ if(I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_BUSY, SET, I2C_TIMEOUT_BUSY_FLAG) != HAL_OK)Another problem is during HAL_I2C_MspInit(I2C_HandleTypeDef* hi2c), after the line /* Peripheral clock enable */__HAL_RCC_I2C2_CLK_ENABLE();you can found setted (in random way) the bit BUSY of register I2C_SR2. Sorry for my english
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-05-06 8:41 AM
Posted on May 06, 2016 at 17:41
Hi,
Could you precise which firmware package are you using ?Locking for BUSY flag as described in the silicon errata in
RegardsOptions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-05-09 7:37 AM
Posted on May 09, 2016 at 16:37
Hi,
1- I2C_TIMEOUT_BUSY_FLAG is predefinied to be 10s (#define I2C_TIMEOUT_BUSY_FLAG ((uint32_t)10000U)) and used to check BUSY flag.However, the parameter ''Timeout'' is used in this check inside the function ''HAL_I2C_IsDeviceReady'': I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_SB, RESET, Timeout). 2- Regarding the second issue (BUSY flag set after enabling I2C clock), try to configure GPIOs and enable alternate functions first, then enable I2C clock.RegardsOptions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-05-10 1:38 AM
Posted on May 10, 2016 at 10:38
Thank you for answer,
i'm using STM32CubeMX 4.14.0Why not put directly inside the initialization code a little fix to solve this problem ?This is your parts of init codeGPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11;GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;GPIO_InitStruct.Pull = GPIO_PULLUP; HAL_GPIO_Init( GPIOB, &GPIO_InitStruct );/* Peripheral clock enable */__HAL_RCC_I2C2_CLK_ENABLE(); // after this line, you can found BUSY flag set also if line of SDA and SCL are high/* Peripheral interrupt init */HAL_NVIC_SetPriority(I2C2_EV_IRQn, 0, 0);HAL_NVIC_EnableIRQ(I2C2_EV_IRQn);HAL_NVIC_SetPriority(I2C2_ER_IRQn, 0, 0);HAL_NVIC_EnableIRQ(I2C2_ER_IRQn);I saw the errata and says to put high interrupt priority for I2C (priority 0) and lower to all others ... I need to reduce the priority also to system tick?About 10 Seconds, you can see inside your function...try to call it with timeout of 100ms and I2C_FLAG_BUSY is set.HAL_StatusTypeDef HAL_I2C_IsDeviceReady(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint32_t Trials, uint32_t Timeout){ uint32_t tickstart = 0, tmp1 = 0, tmp2 = 0, tmp3 = 0, I2C_Trials = 1; if(hi2c->State == HAL_I2C_STATE_READY) { /* Wait until BUSY flag is reset */ if(I2C_WaitOnFlagUntilTimeout(hi2c, I2C_FLAG_BUSY, SET, I2C_TIMEOUT_BUSY_FLAG) != HAL_OK) //10 second of timeout { return HAL_BUSY; }Bye Marco