2017-07-31 6:40 AM
Hi,
I have a Nucleo L053R8, I need of delay of 2 microseconds, but HAL_Delay_Microsecond in NucleoWorkspace not exist.I changed: HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);in HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000000);for use HAL_Delay but the process is blocced.How is can resolved?
2017-07-31 6:55 AM
You can't interrupt at 1 MHz, it just causes the processor to saturate with useless work.
Use a TIM that you have free running at 1 MHz or higher to get some level of precision/granularity, and then delta the TIM->CNT over the period of interest.
2017-08-03 1:32 AM
is strange , if you are not able to use a TIM or HAL_Delay(); use a simply For(i=0,I<65000,i++) according with your MCU Frequency , not a asmart solution make the STM work for that, but might be work.
2017-08-03 1:46 AM
You cannot have a delay of 1 us using Systick timer reason as mentioned above by Clive, maximum that I was able to achieve was 10us using 48Mhz HSE on STM32F0 series. You can use NOP statement and then check the delay on oscilloscope or use TIM.
Regards,Muhammad Moiz khan.2017-08-03 10:06 AM
Hello!
I use it with no problems
Try it..You can change the resolution or change timer to TIM7
APB1_FREQ is the frequency of APB1 timers clock
Init the timer first ..
Not for multithread use
//##############################################################################
void TIM6Init()//as counter only. { RCC->APB1ENR |= RCC_APB1ENR_TIM6EN;//enable clock TIM6->CR2=0;//slave reset TIM6->DIER=0;//interrupts and DMA disable TIM6->SR=0;//clear flag TIM6->EGR=0;//No generate trigger TIM6->CNT=0;//Clear counter TIM6->PSC=APB1_FREQ/1000000-1;// 1 microsecond counter resolution TIM6->ARR=65535;//reload counter full range TIM6->CR1=1;//enable timer }//##############################################################################void DelayMicrosecond(unsigned short microsecond){ TIM6->EGR=1;//reinitialize time counter , prescaler while(TIM6->CNT<microsecond);//wait...}//##############################################################################2017-08-03 12:40 PM
My preference would be for a free-running counter, at higher frequency, not reset/restarted, as this would be both interrupt and thread safe. In non-CM0 cases DWT_CYCCNT is also very effective, being 32-bit and at high rate, and can span multiple seconds (close to a minute at 72 MHz as I recall).
The NOP or for() spin-loops also won't shorten post-interrupt service, and can also be dependent on compiler and optimization selections.
2017-08-03 1:21 PM
It depends the purpose of the microsecond delay, and if it is a min value or not.
For example, a SW delay can easily be tuned using a static variable, you run the SW delay with biggest number within a Systick 1 msec which enables you to calculate the right unit for 2 us. This of course is resource free and has limitations.
HW assisted delays can be done with either timer or even SPI by the time it takes to push a byte without any GPIO wired to it. Numerous solutions exist. If the microsecond delay is used to toggle GPIOs, Timers and their output compare function would make more sense. So... it depends what's for...
2017-09-12 5:16 AM
thanks everybody