cancel
Showing results for 
Search instead for 
Did you mean: 

HAL ccit crc16 for the STM32L15x , is it possible to use the hardware CRC?

gerrie
Associate
Posted on September 09, 2016 at 12:30

I could not find a way to use the HAL (created by cubemx) to calculate a CCIT 16 bit CRC.

I did this for the L476  and this workes

/** -------------------------------------------------------------------------

 * @brief CRC peripheral initialization CRC_POLYNOMIAL_16B

 */

void initialise_crc16_ccit (void)

{

  hcrc.Instance = CRC;

#ifdef STM32L476xx

  // The default polynomial is not used. The one to be used must be defined

    // in CrcHandle.Init.GeneratingPolynomial

  hcrc.Init.DefaultPolynomialUse    = DEFAULT_POLYNOMIAL_DISABLE;

  // Set the value of the generating polynomial.

    // The one used in that example is the 16-bit long CRC generating

    // polynomial X^16 + X^12 + X^5 + 1 */

  hcrc.Init.GeneratingPolynomial    =  CRC_POLYNOMIAL_16B;

  // The user-defined generating polynomial yields a 16-bit long CRC

  hcrc.Init.CRCLength               = CRC_POLYLENGTH_16B;

  // The default initialise value is not used

  hcrc.Init.DefaultInitValueUse     = DEFAULT_INIT_VALUE_DISABLE;

  // User initialise value is used instead

  hcrc.Init.InitValue               = CRC_INIT_VALUE;

  // The input data are inverted by word

  hcrc.Init.InputDataInversionMode  = CRC_INPUTDATA_FORMAT_BYTES;

  // The bit reversal is done on a full word basis.

    // The input stream yielded by CRC16_DATA8[] is the sequence of

    // bytes 0x4D, 0x3C, 0x2B, 0x1A, 0xBE, 0x71, ...

    // meaning that the first word written in the CRC DR register is

    // 0x4D3C2B1A.

    // Bit reversal done by the hardware on the full word leads to the actual

    // CRC processing of

    // 0x58D43CB2.

    //

    // Similarly, the second word written in the IP is 0xBE71C98A, leading to

    // the processing of 0x51938E7D after hardware input data reversal.

    //

    // Note that when the software writes less than a word in the IP (to minimize the

    // number of write accesses for a given number of bytes), the bit-reversal operation

    // is carried out only on the input data.

    // Therefore, the last written data is the last byte 0x5E, processed as 0x7A

    // by the hardware after bit-reversal to wrap-up the CRC computation.

    //

    // This means that the field InputDataInversionMode set to CRC_INPUTDATA_INVERSION_WORD

    // applied to {0x4D, 0x3C, 0x2B, 0x1A, 0xBE, 0x71, 0xC9, 0x8A, 0x5E}

    // yields the same result as InputDataInversionMode set to CRC_INPUTDATA_INVERSION_NONE

    // applied to {0x58, 0xD4, 0x3C, 0xB2, 0x51, 0x93, 0x8E, 0x7D, 0x7A}.

  // The output data are inverted

  hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLED;

  // Output data reversal can only be done at bit level.

    // The expected CRC is 0x5043 after output data reversal, meaning

    // that the CRC before the reversal operation is 0xC20A. */

  // The input data are bytes (8-bit long data)

  hcrc.InputDataFormat              = CRC_INPUTDATA_FORMAT_BYTES;

#endif

#ifdef STM32L151xB

//// @todo Christo we need the CRC for the L151 here

#endif

  // De-initialize the CRC peripheral

  if (HAL_CRC_DeInit(&hcrc) != HAL_OK)

  {

    // Initialization Error

    Error_Handler();

  }

  // Then, initialize the CRC handle

  if (HAL_CRC_Init(&hcrc) != HAL_OK)

  {

    // Initialization Error

    Error_Handler();

  }

}
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Walid FTITI_O
Senior II
Posted on September 09, 2016 at 17:31

Hi de_jager.gerrie,

The CRC calculation unit in STM32F4 is used to get a CRC code in 32 bits data.

For other STM32s like STM32L4 and STM32F3 for example, CRC code is on 8, 16, 32 bits data using a configurable generator polynomial value and size.

In addition to reference manual , you can check the application note ''Using the CRC peipheral in the STM32 family''

http://www.st.com/content/ccc/resource/technical/document/application_note/39/89/da/89/9e/d7/49/b1/DM00068118.pdf/files/DM00068118.pdf/jcr:content/translations/en.DM00068118.pdf

-Hannibal-