2025-12-16 10:25 PM
Hello STM32 Community,
I am a newbie and facing an issue with my NUCLEO-STM32H755ZI board.
I am unable to connect to the STM32H755 target using STM32CubeProgrammer, even though the ST-LINK appears to be working correctly,
Board: NUCLEO-STM32H755ZI
Debugger: On-board ST-LINK
USB connection: CN1 (USB-A to Micro-B).
ST-LINK is detected correctly by Windows
ST-LINK Virtual COM Port is visible in Device Manager
Target voltage ~3.27 V is shown in Cube programmer.
Green power LED (LD3) is
2025-12-16 10:35 PM
Hi,
Did it work before? Did you flash anything?
Try connecting with setting: hardware reset.
Did you change/set the power supply setting?
Maybe then need start the bootloader by setting the boot0 high and then power up with dfu mode to recover to a working state.
2025-12-17 2:45 AM
@AScha.3 wrote:Did you change/set the power supply setting?
@Renee - see: How to unbrick an STM32H7 after setting the wrong power mode.
Also, for general debugger connection issues:
How to solve connection errors when connecting and programming the STM32 target board.
How to solve debugger connection issues.