2016-01-26 11:03 AM
Hello. I try to make a simple non-continuous ADC-DMA transaction of 10 measurements. I get only one sample in my array. I don't use interrupts, just wait for DMA completion. Could you tell, what I am doing wrong?
Here are my functions (I am sorry if there exist some codebox tag and I did not notice it): UINT16 Adc1ShortReadBuf[10]; void Get10Samples(void) { DMA_HandleTypeDef DmaHandle1; DmaHandle1.Init.Channel = DMA_CHANNEL_0; DmaHandle1.Instance = DMA2_Stream4; HAL_DMA_DeInit(&DmaHandle1); DmaHandle1.Init.Direction = DMA_PERIPH_TO_MEMORY; DmaHandle1.Init.PeriphInc = DMA_PINC_DISABLE; DmaHandle1.Init.MemInc = DMA_MINC_ENABLE; DmaHandle1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; DmaHandle1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; DmaHandle1.Init.Mode = DMA_NORMAL; DmaHandle1.Init.Priority = DMA_PRIORITY_HIGH; DmaHandle1.Init.FIFOMode = DMA_FIFOMODE_DISABLE; DmaHandle1.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_HALFFULL; DmaHandle1.Init.MemBurst = DMA_MBURST_SINGLE; DmaHandle1.Init.PeriphBurst = DMA_PBURST_SINGLE; HAL_DMA_Init(&DmaHandle1); ADC_ChannelConfTypeDef sConfig; sConfig.SamplingTime = ADC_SAMPLETIME_112CYCLES; sConfig.Rank = 1; sConfig.Offset = 0; ADC_HandleTypeDef AdcHandle1; ADC_MultiModeTypeDef multimode; AdcHandle1.Instance = ADC1; HAL_ADC_DeInit(&AdcHandle1); AdcHandle1.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV8 ; AdcHandle1.Init.Resolution = ADC_RESOLUTION12b; AdcHandle1.Init.ScanConvMode = DISABLE; AdcHandle1.Init.ContinuousConvMode = DISABLE; AdcHandle1.Init.DiscontinuousConvMode = DISABLE; AdcHandle1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; AdcHandle1.Init.ExternalTrigConv = ADC_SOFTWARE_START; AdcHandle1.Init.DataAlign = ADC_DATAALIGN_RIGHT; AdcHandle2.Init.NbrOfDiscConversion = 0; AdcHandle1.Init.NbrOfConversion = 1; AdcHandle1.Init.DMAContinuousRequests = DISABLE; AdcHandle1.Init.EOCSelection = DISABLE; HAL_ADC_Init(&AdcHandle1); multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_5CYCLES; multimode.Mode = ADC_MODE_INDEPENDENT; multimode.DMAAccessMode = ADC_DMAACCESSMODE_DISABLED; HAL_ADCEx_MultiModeConfigChannel(&AdcHandle1, &multimode); DMA_ClearTCFlag(&DmaHandle1); sConfig.Channel = ADC_CHANNEL_0; HAL_ADC_ConfigChannel(&AdcHandle1, &sConfig); __HAL_LINKDMA(&AdcHandle1, DMA_Handle, DmaHandle1); ADC_DMA_start(&AdcHandle1, (uint32_t*)Adc1ShortReadBuf, 10); } HAL_StatusTypeDef ADC_DMA_start(ADC_HandleTypeDef* hadc, uint32_t* pData, uint32_t Length) { __IO uint32_t counter = 0; /* Enable ADC DMA mode */ hadc->Instance->CR2 |= ADC_CR2_DMA; /* Set src and dst addresses and length*/ HAL_DMA_Start(hadc->DMA_Handle, (uint32_t)&hadc->Instance->DR, (uint32_t)pData, Length); /* Check if ADC peripheral is disabled in order to enable it and wait during Tstab time the ADC's stabilization */ if((hadc->Instance->CR2 & ADC_CR2_ADON) != ADC_CR2_ADON) { /* Enable the Peripheral */ __HAL_ADC_ENABLE(hadc); /* Delay for ADC stabilization time */ /* Compute number of CPU cycles to wait for */ counter = (ADC_STAB_DELAY_US * (SystemCoreClock / 1000000)); while(counter != 0) { counter--; } } hadc->Instance->CR2 |= ADC_CR2_SWSTART; /* Return function status */ return HAL_OK; } Solved it. Conversion has to be continuous. Actually, the post can be deleted. AB2016-01-28 2:14 AM
Hi baranov.aleksandr,
I don't agree to delete the post.It should be kept to help other users that may face same issue.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.