2025-02-10 11:18 PM - edited 2025-02-10 11:21 PM
Hi all,
i have an issue with an STM32-H7A3, which is going into hard fault, when calling a function, which is moved to the ITCM-RAM.
I have defined a section for ITCM-RAM in the Linker-Script:
_siitcmram = LOADADDR(.itcmram); /* size of ITCM-RAM */
.itcmram : { /* ITCM-RAM Section */
. = ALIGN(4); /* Alignment: 4 Bytes - "Word" - u32 */
_sitcmram = .; /* define a global symbols at itcmram start */
*(.itcmram)
*(.itcmram*)
. = ALIGN(4);
_eitcmram = .; /* define a global symbols at itcmram end */
} >ITCMRAM AT> FLASH /* reseve memory in flash for this section */
I copy the code from the flash to the ITCM-RAM in the startup
// BEGIN MODIFICATION - STM-CubeMX Code above
/* Copy from flash to ITCMRAM */
ldr r0, = _sitcmram // start: itcmram start
ldr r1, = _eitcmram // end: itcmram end
ldr r2, = _siitcmram // size
movs r3, #0
b LoopCopyCCMInit
CopyCCMInit:
ldr r4, [r2, r3]
str r4, [r0, r3]
adds r3, r3, #4
LoopCopyCCMInit:
adds r4, r0, r3
cmp r4, r1
bcc CopyCCMInit
/* End of copy to ITCMRAM */
// END MODIFICATION - STM-CubeMX Code below
basically the code above is just a "Copy & Paste" of the section above, where the data get copied from Flash to RAM. I Just edited the names and symbols.
I got the same ruinning - with the same functions - in a Test Project without any issues. The only issue I had at the beginning in the test project was, that I did not copy the code from flash to the ITCM-RAM, but when I did that it worked as intended.
But in this case i can litterally see, that somthing is wrong, because when I step through my code in the debugger, I can not jump (with "step into (F5)") into the function. The debugger simply steps over and quickly goes into hard fault. So my asumption is: for some reason the code is not copied into the ITCMRAM, and the copied functions seem to have the address 0x00 - which is the reason why it goes into hard fault quickly.
Obviously I am missing something. But I don't know what. Can anyone help me out?
Additional Info:
In the CubeIDE Memory Details, I can see the code that should be in the ITCM-RAM is allocated in the ITCM-RAM. There is also a ITCM-RAM section in the flash, where the code that gets copied is stored.
2025-02-11 12:19 AM
2025-02-11 12:47 AM
thanks for the input. It's a nice tutorial to explain how to use the ITCM-RAM.
If it is your tutorial I have 2 comments:
a) typo the 3rd line, the ITCM RAM has 16 kB not 16 MB
b) i wonder how the tutorial works without copying the flash contents into the ITCM-RAM? AFAIK this is "mandatory" to copy the ITCM-Code from the Flash into the ITCM-RAM at the startup ...
but I used your input to check the Memory in the Memory Viewer. And the result is: the whole ITCM-RAM starting at 0x00 seems to be full with random data. This means my code in the startup script somehow has no effect. The same code is working in another project on the same Nucleo, and I wonder why it works in one build but not in another? Thats weird ...
2025-02-11 01:00 AM
I don't have a H7 device, nor I'm really experienced with this variants.
However, two points you might consider.
First, I assume the code you copy is linked for this address, or PIC.
And second, the issues might be related to clock / system setup. I had similiar issues with external RAM, which is of course a different matter.
But perhaps you can try to copy the code after the setup.
Another possible reason might be the MPU, if you use it in your application.