cancel
Showing results for 
Search instead for 
Did you mean: 

GPIO ODR Register

Sean Mutlu
Associate II
Posted on July 09, 2017 at 20:32

Hello, 

Was doing some tests with the ODR register for GPIO and noticed that when I load it with 0xFFFF some pins (13-15 for GPIOA &GPIOC) were still off. I have them initialized so I am unsure why they won't come on. Wondering why this happens and how to overcome this. Also might there be an easier/faster/less trivial way to initialize all pins to the same for GPIOA/B/C?

Source Code:

&sharpinclude 'stm32f10x_gpio.h'

&sharpinclude 'stm32f10x_rcc.h'

GPIO_InitTypeDef GPIO_InitStructure;

int main(void)

{

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA,ENABLE);

GPIO_StructInit(&GPIO_InitStructure);

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0|GPIO_Pin_1|GPIO_Pin_2|GPIO_Pin_3|GPIO_Pin_4|GPIO_Pin_5|GPIO_Pin_6|GPIO_Pin_7|GPIO_Pin_8|GPIO_Pin_9|GPIO_Pin_10|GPIO_Pin_11|GPIO_Pin_12|GPIO_Pin_13|GPIO_Pin_14|GPIO_Pin_15;

GPIO_Init(GPIOA,&GPIO_InitStructure);

while(1)

{

GPIOA->ODR = 0xFFFF;

}

}

#odr #gpio
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on July 09, 2017 at 23:25

What do they connect to externally? PA13 and PA14 would nominally be used by the debug interface.

PC13,14 and 15 are typically in the low power domain, so don't have high current drive capabilities.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on July 10, 2017 at 01:07

Just an LED which i was using to probe all outputs, I may have misunderstood this register, i thought it loaded all 16 bits to output of respective port.

Posted on July 10, 2017 at 01:08

By that i meant I am under the impression that:

GPIOA->ODR = 0xFFFF;

should make every port (0-15) in GPIOA high

Posted on July 10, 2017 at 02:31

It should, you'd want to read back the mode settings.

IDR should always reflect the pin state, ODR will drive those pin set as outputs. Potential for pins to clash with external circuitry, driving an alternate state, or pins shorted on the board.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..