cancel
Showing results for 
Search instead for 
Did you mean: 

GNU ARM Eclipse is now available from Eclipse Marketplace

Liviu Ionescu
Associate III
Posted on December 09, 2015 at 15:11

Overview

The 

https://github.com/gnuarmeclipse

 includes a set of open source Eclipse plug-ins and tools to create/build/debug/manage 

ARM

(32-bits) and 

AArch64

 (64-bits) applications and static/shared libraries, using the latest 

GNU ARM GCC

 toolchains. 

Eclipse Marketplace

Aiming to further improve the user experience while installing/updating the plug-ins, the 

GNU ARM Eclipse

 project was registered to 

https://marketplace.eclipse.org/content/gnu-arm-eclipse

:

0690X00000604t9QAA.png

Benefits

The main advantage of using the Eclipse Marketplace is a 

simplified install procedure

, no longer requiring to manually enter the update site address.

The Install button

The Eclipse Marketplace not only provides a centralised index to locate projects, it goes one step further and provides a drag-and-drop browser button.

0690X00000604tJQAQ.png

As seen above, the button can be included in any web page.

To use it, just 

drag-and-drop the button to a running Eclipse

, and the plug-ins to install/update will be automatically identified:

0690X00000604tTQAQ.png

If, for any reason, this does not work, it is always possible to search the Eclipse Marketplace manually from within Eclipse menus:

0690X00000604tOQAQ.png

More info

For more details about the 

GNU ARM Eclipse

 project, please refer to the project site 

http://gnuarmeclipse.github.io/

.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0