2008-04-09 11:38 PM
Flashlink/STM3210B-eval
2011-05-17 3:28 AM
Hi everybody...
I found today my old FlashLink JTAG programmer used for the DK3200 evaluation board of a µPSD3200.I have all the JTAG output wire by wire on this interface. I will buy STM3210B-eval board this week and i have a question. Can i download program and maybe Debug it on the STM32 eval board with my FlashlinkJtag from ST? This flashlink is plug on the PC by paralel port and i'm using Ride7. I have an other question too. There is somebody here who has already use the EMBEDED Rlink of the Raisonance starter kit to download and debug program on the ST evaluation board ? I know my questions are long ....sorry...but i will be glad to have more information about these problems . Thank you very much :D2011-05-17 3:28 AM
Hello,
I beleive that you were using FlashLink with CAPS or JTAG programmer tool to load applications on STR9/µPSD boards. For the moment the CAPS tool does not support the STM32 devices. Were you using Flashlink with other toolchains? Concerning the RLINK, you can use it with the RIDE7, RIDE6 or Rflasher and STM32 devices. you have just to detach it from the REva board. What is the starter kit you have (STR7, STR9...) Any way, the attached document would be helpful (section 1.2) Best Regards, Ibtissem. [ This message was edited by: ibtissem.malouche on 10-04-2008 12:15 ]