cancel
Showing results for 
Search instead for 
Did you mean: 

Executing binaries

daviddavid92
Associate II
Posted on May 20, 2010 at 13:36

Executing binaries

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on May 17, 2011 at 13:51

ELF would be the way to go, perhaps overkill, but the tools generate it and it is well documented.

You should probably look at the linker (and the directive file) rather than the compiler. The objects emitted by the compiler are relocatable ELF objects. You might look at the --emit-relocs option to keep them.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
sjo2
Associate III
Posted on May 17, 2011 at 13:51

-fpic does work, but you will have to handle the GOT - been a while and i was only executing small amounts of code.

also maybe of interest:

http://nuttx.sourceforge.net/NuttXNxFlat.html

Cheers

Spen

daviddavid92
Associate II
Posted on May 17, 2011 at 13:51

Helpful - thanks!

Chris.