cancel
Showing results for 
Search instead for 
Did you mean: 

Error: L6218E: Undefined symbol SystemInit (referred from startup_stm32f10x_hd.o)

mircead2011
Associate
Posted on June 24, 2014 at 17:08

Hi.

I try to make a simple program using a STM32F013ZE microcontroller, but i receive the next error : 

''.\Blink four LEDs.axf: Error: L6218E: Undefined symbol SystemInit (referred from startup_stm32f10x_hd.o).

Not enough information to list image symbols.''

Program code : 

&sharpinclude<stm32f10x.h>                          // STM32F103 definitions

void wait();

int main (void) 

{

unsigned int i;                                 // LED variable

RCC->APB2ENR |= (1UL << 7);    // Enable GPIOF, GPIOC, GPIOB clock

GPIOF->CRL    =  0x33000000;     // PF.6, PF.7 defined as Outputs   

GPIOF->CRH    =  0x33;                  // PF.8, PF.9 defined as Outputs

while (1)  

{                                    

for(i = 1<<6; i < 1<<10; i <<= 1) 

{    

GPIOF->BSRR = i;          // Turn LED on

wait();                                // call wait function

GPIOF->BRR = i;             // Turn LED off

}

}

}

void wait(void)  

{

int  d;

for(d = 0; d < 1000000; d++);               // only to delay for LED flashes

}

#gpio #stm32
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0