cancel
Showing results for 
Search instead for 
Did you mean: 

EEPROM writing operation optimization ?

tingting
Associate II
Posted on February 12, 2016 at 15:32

Hi,

I am using STM32L051, I need to write a big amount of data (200 bytes) in the memory .

Today this operation takes about 1,4s . But it is too slow .

In the RM0377(page 71), there should be a means to write a half page with only one waiting time.

Is there an example code for that?

Thank you !
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0