cancel
Showing results for 
Search instead for 
Did you mean: 

Durability of 80-byte User Memory in Backup Domain of STM32F405

majorbulk
Associate
Posted on July 22, 2012 at 03:26

Greetings,

I have a small number of bytes (less than 80 bytes) that I need to store in persistent storage, but the values may change in excess of 10,000 times.  I believe the SRAM would work fine for this, but I would rather not use the extra battery power to maintain the SRAM if the 80-byte memory in the backup domain can handle the write frequency I anticipate.  What kind of memory is this 80-byte user memory?  What are the specs for number of writes? 

Thanks,

Valkyrie-MT

#sram-backup-rtc
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jpeacock2399
Associate II
Posted on July 23, 2012 at 16:02

The backup registers are SRAM powered from the backup (Vbat) power domain.  For the STM32F1xx series these are 16-bit half words; don't try to use 32-bit access.  You will need a battery or some other backup supply (i.e. supecap) in order to save data in the backup registers.  Be aware that a tamper event (if you have it enabled) will erase the 80 byte backup register area.

  Jack Peacock

majorbulk
Associate
Posted on July 24, 2012 at 06:28

Excellent!  Exactly the answer I was hoping for!  And thanks for the tip on the tampering.  I'll have to figure out how to disable that. 

-Valkyrie-MT