cancel
Showing results for 
Search instead for 
Did you mean: 

Dual regular simultaneous mode with DMA

Florian Braun
Associate
Posted on May 29, 2017 at 17:16

Hello everybody.

I want to sample A0 (ADC1) and A1 (ADC2) in the dual regular simultaneous mode (Trigger Timer 2).

So I have created a Project with cubemx (Nucleo-F446RE) and HAL-Libary.

The Problem is that the conversion starts only one time. So if I change the potentiometer the value from the ISR-Variable is not update.

Maybe someone have got more experiance with this ADC-mode an can help me!

Thanks,

Flo

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0