cancel
Showing results for 
Search instead for 
Did you mean: 

dspin discovery example project for IAR

apfrancia
Associate
Posted on June 11, 2014 at 10:00

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
frankmeyer9
Associate II
Posted on June 11, 2014 at 10:38

Perhaps the project was created with/for another version of the IAR toolchain (assuming it was not hastily setup in a bad manner by ST).

The missing include files would be easy to fix.

Just add the appropriate folders to the include search path list in the GUI (I'm no IAR user ...).

The project 'fwlibraries dspin discoverykit' contains the unknown tool 'CMSISDAP_ID'

 

The project 'fwlibraries dspin discoverykit' contains the unknown tool 'IJET_ID

 

That looks like environment variable definitions that are expected to contain the name/path of some tool. CMSIS-DAP is the debug interface used at Freescale's FRDM boards, so I guess you don't need that.