cancel
Showing results for 
Search instead for 
Did you mean: 

Drivers for MAX30102/30100 and Protocentral MAX86150 on STM32L475VGT6

Anuraag
Visitor

Hello,

I’m using the STM32L475VGT6 board and need drivers for the MAX30102/MAX30100 and Protocentral MAX86150 sensors. I couldn’t find official or compatible drivers for these sensors on this MCU.

If anyone has links to drivers, example code, or advice on integration with STM32L475VGT6 (using STM32CubeIDE or HAL libraries), please share.

Thanks in advance!

0 REPLIES 0