cancel
Showing results for 
Search instead for 
Did you mean: 

Does ST Microelectronics have SiP chips? Microcontrollers with built in Bluetooth?

Sashvat
Associate II

Hello everyone i was wondering if STM sold microcontrollers with bluetooth integrated into it. Please do let me know the names of the chips

Thank you

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Peter BENSCH
ST Employee

You will find all MCUs with wireless connectivity here. There is also the STM32WB family of devices that contain a Bluetooth radio module.

Good luck

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

So can i use this microcontroller without any extra hardware for the bluetooth? (Except for some antenna and an inductor) can i use it like those arduino modules you get and program them straight away without needing much extra hardware?

Peter BENSCH
ST Employee
Well, there are several options, but it sounds like you need a ready-made module. For this the module BlueNRG-M2 might be one option, because it already contains everything including the antenna:
https://www.st.com/en/wireless-connectivity/bluenrg-m2.html
Another one is the dual-core module STM32WB5MMG:
https://www.st.com/en/microcontrollers-microprocessors/stm32wb5mmg.html
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks for suggesting me this, but i am trying to keep my pcb as small as possible so what must i do to use the bluetooth on the STM32WB chips? i have chosen the STM32WB55CCU7, is it more like designing a bluetooth module from scratch? or is it something where i have to just add a few components?