cancel
Showing results for 
Search instead for 
Did you mean: 

Do I have to use STM32 HAL for Keil uvision Run Time Environment ( Device start up File

AElah.1
Associate

I am Using STM32L152 with Keil uvision5 and for setup Run Time Environment must selct STM32cube HAL library, do I have to use HAL or I can use only device start up

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
FBL
ST Employee

Hello @AElah.1​,

Indeed, it is possible to use device's startup file. However, It is recommended to use HAL for ease of use and functionalities.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL