2025-03-10 8:12 AM
Hi all,
I'm quite a beginner with these kind of memories. It seems that the ST Core Coupled Memory is inspired in the ARM's Tightly coupled memory concept, however, do they have a significant difference? Perhaps a special Hardware adapation to ST's Microprocessor architecture or something similar?
Thanks in advance.
2025-03-10 9:02 AM
ARM Cortex-M4 does not feature TCM by ARM, instead CCM was added for some F3, F4, G4 MCUs by ST.
The goal is the same: 0-wait state access.
Look at the block diagram of the chip/series you are interested in:
How is the RAM connected? Data Bus, Instruction Bus, both? separate I-TCM and D-TCM?
Is DMA access possible?
hth
KnarfB