cancel
Showing results for 
Search instead for 
Did you mean: 

DfuSe doesn't work

Linda
Associate II
Posted on January 26, 2015 at 01:42

I down load a DfuSe demo, but it can not read a *.hex file.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Posted on January 26, 2015 at 03:25

The DFU Manager 3.04 has issues as I recall, you'd need to use an older version.

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/DFU%20File%20Manager%20Unable%20to%20create%20image%20from%20this%20file&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=248]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FDFU%20File%20Manager%20Unable%20to%20create%20image%20from%20this%20file&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=248

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Linda
Associate II
Posted on January 26, 2015 at 04:23

Dear Sir,

I down load and try both of 3.0.2 and 3.0.3, reading file there is no problem, but window can not detect this STM board even though I have put the BOOT0 to VDD.

I read the readme.txt, it should :

~~~~~~~~~~~~~~~

 3- Install your device with the driver and the inf file

~~~~~~~~~~~~

I couldn't find the driver and inf file in the package. Where I can get it?

Thanks  a lot

Posted on January 26, 2015 at 04:58

Maybe there are other issues? If you can't see it in Device Manager, it's not connecting at all.

C:\Program Files (x86)\STMicroelectronics\Software\DfuSe\Driver ?? 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Linda
Associate II
Posted on January 27, 2015 at 21:25

The PC only find STMicroelectronics STLink dongle all the time. even I delete and restart the computer, it just can not find the STM32F4 Doese the Dfuse work with STM32F429?

Thanks

Posted on January 27, 2015 at 21:45

The PC only find STMicroelectronics STLink dongle all the time. even I delete and restart the computer, it just can not find the STM32F429. Does the Dfuse work with STM32F429?

I don't recall. It would be the other USB connector, not the ST-LINK one, but the STM32F429I-DISCO does use the HS USB port, not the FS USB port like the STM32F4-DISCO. What does the System Loader say about pins/ports? This would be the controlling document as to what will/will not work.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..