cancel
Showing results for 
Search instead for 
Did you mean: 

DEV_TARGET_CMD_ERR on breakpoints (Rowley Crossworks)

kk6gm
Associate II
Posted on May 30, 2011 at 01:57

I've just gotten some STM32VLDiscovery boards and am attempting to program them via Rowley Crossworks.  I've got the STLink connection working and can download and run programs and view registers, etc.  But if I try to set a breakpoint, when that breakpoint is hit I get the above error (DEV_TARGET_CMD_ERR) and, FWIW, both Discovery red LEDs go solid ON.  Does this describe any known issue?  Any hints as to what may be going wrong?  I've tried multiple boards so hardware is ruled out.

BTW, the version of stlinkusbdriver.dll I'm using, from the ST website, is 4.0.1b.  Any known problems with that?
2 REPLIES 2
kk6gm
Associate II
Posted on June 01, 2011 at 05:28

OK, problem solved (or at least, disappeared).  I made a new project using the same source files to send to Rowley, built it and just tried it for the heck of it, and it works.  Good, now I can play.

bbenjamin
Associate
Posted on August 03, 2011 at 23:56

I had this same problem and found that deleting the not found symbols in the Watch window allows breakpoints to work. I've posted this up on Rowley's forum.