cancel
Showing results for 
Search instead for 
Did you mean: 

detecting edge in falling/rising mode interrupt

fatemehjml
Associate II
Posted on July 23, 2014 at 11:10

I want to config external interrupt line 0 in both falling/rising edge mode. But I don't know how I can detect that event happen due to falling edge or rising edge. It should do different function for falling and rising edge.

 I can't use two external interrupt pin and connect them to find every rising or falling edge.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0