cancel
Showing results for 
Search instead for 
Did you mean: 

DCMI max transfer rate

armindavatgaran
Associate III
Posted on January 24, 2017 at 19:28

Hello

It is mentioned in the table 87 (DCMI characteristics, stm32f405/407 datasheet, Rev7) that max DCMI_PIXCLK is 54 MHz, and it's mentioned in the RM0090 that this peripheral is capable of up to 54MBytes/s transfer rate. The question is, how number of data lines affects this throughput rate? is this rate just for 8 data lines (because of that it uses whole of data register)?

Thanks.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Amel NASRI
ST Employee
Posted on January 25, 2017 at 11:35

Hi

tag.aseok

‌,

For the same datasheet table (

DCMI characteristics), it is specified that configuration used 'Data format: 14 bits'.

Referring to RM0090, we have the following:

- 8-bit data: 'to capture a 32-bit word, the camera interface takes four pixel clock cycles.'

- 10/12/14-bit data: ' a 32-bit data word is made up every two pixel clock cycles'

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on February 10, 2017 at 06:28

Hello, according to that table, 54MHz * (7/4 Bytes) = 94.5 MBytes/s. Is it correct?