cancel
Showing results for 
Search instead for 
Did you mean: 

DAC Audio Signal Profile

benjaminsasseen9
Associate
Posted on August 04, 2010 at 20:09

DAC Audio Signal Profile

1 REPLY 1
raptorhal2
Lead
Posted on May 17, 2011 at 14:00

The DAC will put out 0 volts for a DAC output register value = 0 and DAC reference voltage (usually 3.3 volts) for a DAC output register = 4095, and intermediate voltages for intermediate register values.

Sound occurs when a sequence of numbers is converted to a voltage to produce a changing waveform. So when the DAC register doesn't change (at any value), the speaker is not vibrating, so there is no sound.

Your challenge is to find out what range of numbers is coming out of the wave file and rescale if necessary to fit the 8 or 12 bit DAC range so you get reasonable accuracy without clipping.

Cheers, Hal