cancel
Showing results for 
Search instead for 
Did you mean: 

D flip-flop

PKurz.1
Associate II

Hi,

I need to normalize the asynchronous transmission to a specific baudrate in real time. I know flip-flop D is fine, but I don't want to add extra elements to the layout. Can I do it with timers or maybe some other solution?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

TIM can modulate all kinds of signals.

The STM32 pins have an input synchronize, which is probably a three-stage flip-flop arrangement.

As I recall that's at the TIMCLK, but has some other filter settings. Perhaps the timer cook-book has some specifics?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User

What is the source of asynchronous transmission and what exactly do you mean by "normalize" in this context? A diagram would probably help.

JW

The signal source is the LF antenna connected to the comparator. Then the signal goes to the timer which works in OPM mode. Works as an envelope detector. Duration of high / low depending on signal strength. The baud rate is known and I want the high / low signal to persist according to this speed.