cancel
Showing results for 
Search instead for 
Did you mean: 

Current consumption and state of GPIO in StandBy mode?

Vu.Andy
Associate III
Posted on November 11, 2016 at 18:35

For the STM32F0 device, in the standby mode after executing the function HAL_PWR_EnterSTANDBYMode(), will all the GPIO pins (except for the wakup pin and RTC tamper ...) are put in highZ mode?  Or is it something I have to explicitly do in the codes?

Also, assuming all the GPIO pins are in highZ mode, based on the datasheet, the current consumption for the following are in worse case:

Idd = 3.1uA

Idda = 4.6uA

RTC = 2.8uA

Are these accurate?  Are there any other source of current I should take into account?

Thanks.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0