cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX STM32L433CC bug?

nichtgedacht
Senior
Posted on February 07, 2017 at 17:36

Hi

CubeMX generates the following code for a timer (timer2) with 4 PWM channels.

Each of the channels are configured with the same parameters.

Obviously for channel1 the line:

GPIO_InitStruct.Alternate = GPIO_AF1_TIM2;

is missing. Timer2 channel 1 do not work before inserting this line by hand.

void HAL_TIM_MspPostInit(TIM_HandleTypeDef* timHandle)
{
GPIO_InitTypeDef GPIO_InitStruct;
 if(timHandle->Instance==TIM1)
 {
 /* USER CODE BEGIN TIM1_MspPostInit 0 */
/* USER CODE END TIM1_MspPostInit 0 */
 /**TIM1 GPIO Configuration 
 PA8 ------> TIM1_CH1 
 */
 GPIO_InitStruct.Pin = GPIO_PIN_8;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF1_TIM1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* USER CODE BEGIN TIM1_MspPostInit 1 */
/* USER CODE END TIM1_MspPostInit 1 */
 }
 else if(timHandle->Instance==TIM2)
 {
 /* USER CODE BEGIN TIM2_MspPostInit 0 */
/* USER CODE END TIM2_MspPostInit 0 */
 
 /**TIM2 GPIO Configuration 
 PA0 ------> TIM2_CH1
 PA1 ------> TIM2_CH2
 PB10 ------> TIM2_CH3
 PB11 ------> TIM2_CH4 
 */
 GPIO_InitStruct.Pin = GPIO_PIN_0;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_1;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF1_TIM2;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF1_TIM2;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* USER CODE BEGIN TIM2_MspPostInit 1 */
/* USER CODE END TIM2_MspPostInit 1 */
 }
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

BTW How can one format source code in postings at st.com?

Everything which I tried results in a mess.

There should be a preview option also.

Regards

Dieter

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Jeanne Joly
Senior III
Posted on March 20, 2017 at 09:35

Hello

Br_ggemann.Dieter

,

This issue will be corrected in the next CubeMX release (4.21).

This next release will come soon!

BR. Eric