Question
CubeMX Feature request: set log level on command line
Posted on February 18, 2018 at 12:09
Hello,
I'm using cubeMx with command line and scripts as part of my build process . That's really usefull.
But CubeMx generates a lot of log informations that are certainaly usefull for cubeMx developers but not that much
for anybody else if everything goes right. These informations pollute the build log file.
Would be cool to have the opportunity to turn a switch on the command line to set the log level.
Thanks for you attention.
Julien