cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 4.25.0 bug report

Istvan Nagy
Associate
Posted on March 22, 2018 at 18:54

Hello!

I have just updated CubeMX to 4.25.0 but none of the generated codes work within Keil. If i use code from older projects which were made by CubeMX 4.24 ,they work flawlessly but if i generate a simple initialization code with CubeMX and try even blink a LED on STM32L476 Discovery board it does not work.

Did anyone notice some troubles with the update?

int main(void)

{

  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration----------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */

  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */

  MX_GPIO_Init();

  MX_I2C1_Init();

  MX_I2C2_Init();

  MX_LCD_Init();

  MX_QUADSPI_Init();

  MX_SAI1_Init();

  MX_SPI2_Init();

  MX_USART2_UART_Init();

  MX_USB_HOST_Init();

  /* USER CODE BEGIN 2 */

  /* USER CODE END 2 */

  /* Infinite loop */

  /* USER CODE BEGIN WHILE */

  while (1)

  {

        HAL_Delay(300);

        HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_2);

  /* USER CODE BEGIN 3 */

  }

  /* USER CODE END 3 */

}

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Tim Wuu
Associate
Posted on March 31, 2018 at 07:51

If you are using PLL, it's probably it's missing

RCC_OscInitStruct.PLL.

PLLM in 

SystemClock_Config().

Posted on April 25, 2018 at 16:39

Hi Istvan,

Thanks for your feedback and sorry for late response.

To figure out this issue, can you please specify your:

  • Keil version.

  • STM32Cube FW_L4 version.

Additionally, it will be more helpful if you share your CubeMX project (.ioc) 

Thanks in advance for helping to complete this thread.

Best Regards,

Mohamed

NamSoo Kim
Associate

I have the same problem..

CubeMX 4.26.1(STM32Cube_FW_L1_V1.8.1) + STM32L152CDISCO board

MX_LCD_Init()

HAL_StatusTypeDef HAL_LCD_Init(LCD_HandleTypeDef *hlcd)

.

.

.

 /*!< Wait Until the LCD Booster is ready */

 while(__HAL_LCD_GET_FLAG(hlcd, LCD_FLAG_RDY) == RESET)

 {

  if((HAL_GetTick() - tickstart ) > LCD_TIMEOUT_VALUE)

  {  

   hlcd->ErrorCode = HAL_LCD_ERROR_RDY;  

   return HAL_TIMEOUT;

  } 

 }

HAL_TIMEOUT error!!!