cancel
Showing results for 
Search instead for 
Did you mean: 

CubeF0: Clock mode not configured in LL ADC driver

Miguel Cabrita
Associate II
Posted on May 30, 2018 at 13:38

Hi everyone,

I'm sorry to push this old thread but I'm facing problems using the LL drivers and initializing the ADC.

The function LL_ADC_Init(ADC_TypeDef *ADCx, LL_ADC_InitTypeDef *ADC_InitStruct) doesn't set the CKMODE in ADC_CFGR2.

Does anyone else also have this problem?

Best regards

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee
Posted on May 30, 2018 at 15:47

Hi

Cabrita.Miguel

‌,

I confirm thatLL_ADC_Init has to be updated in order to set the correct value in ADC_CFGR2 depending on selected clock source.

This issue is reported to our development team.

As workaround, I suggest you may set ADC clock with a call of 'LL_ADC_SetClock'.

Ex:LL_ADC_SetClock(ADC1, LL_ADC_CLOCK_SYNC_PCLK_DIV2);

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Amel NASRI
ST Employee
Posted on May 30, 2018 at 15:47

Hi

Cabrita.Miguel

‌,

I confirm thatLL_ADC_Init has to be updated in order to set the correct value in ADC_CFGR2 depending on selected clock source.

This issue is reported to our development team.

As workaround, I suggest you may set ADC clock with a call of 'LL_ADC_SetClock'.

Ex:LL_ADC_SetClock(ADC1, LL_ADC_CLOCK_SYNC_PCLK_DIV2);

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on June 07, 2018 at 18:21

Hi Amel,

thank you for confirming this issue. I'm looking forward to the update

Best regards