CS43L22 play-out is not working
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-02-22 1:24 AM
Posted on February 22, 2016 at 10:24
I copied the CS43L22's schematic design from STM32F4-DISCOVERY. There is only 1 point different in my circuit (a mistake during design) that is VP, VL is 3.3V instead of 3V like STM32F4-DISCOVERY. As per the datasheet of CS43L22, 3.3V is in the working range.
my MCU is able to read\write the control registers on CS43L22 via I2C.However, I almost don't receive any audio output form CS43L22.I have measured the signals input of CS43L22 : MCLK, SCLK, SDIN,LRCL. And I see they are fine.I have streamed my microphone data to USB to verify the audio signal and it is also fine.anyone can help me to show this problemThank you!
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0