cancel
Showing results for 
Search instead for 
Did you mean: 

Counting impulses with LPTIM2 on STM32L487 in STOP2

Jakub Konieczny
Associate II
Posted on July 14, 2017 at 10:45

Hi. I'm trying to count impulses on LPTIM2 in STOP2 mode.

Enabe clocks:

        LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOC);

        LL_RCC_SetLPTIMClockSource(LL_RCC_LPTIM2_CLKSOURCE_LSE);

        LL_APB1_GRP2_EnableClock(LL_APB1_GRP2_PERIPH_LPTIM2);

Configuring PC0 pin:

        LL_GPIO_SetPinMode(GPIOC, LL_GPIO_PIN_0, LL_GPIO_MODE_ALTERNATE);

        LL_GPIO_SetAFPin(GPIOC, LL_GPIO_PIN_0, LL_GPIO_AF_14);

        LL_GPIO_SetPinSpeed(GPIOC, LL_GPIO_PIN_0, LL_GPIO_SPEED_FAST);

        LL_GPIO_SetPinOutputType(GPIOC, LL_GPIO_PIN_0, LL_GPIO_OUTPUT_PUSHPULL);

        LL_GPIO_SetPinPull(GPIOC, LL_GPIO_PIN_0, LL_GPIO_PULL_NO);

Configuring LPTIM2:

        LL_LPTIM_SetAutoReload(LPTIM2, 0xFFFF);

        LL_LPTIM_SetClockSource(LPTIM2, LL_LPTIM_CLK_SOURCE_EXTERNAL);

        LL_LPTIM_SetPrescaler(LPTIM2, LL_LPTIM_PRESCALER_DIV1);

        LL_LPTIM_SetPolarity(LPTIM2, LL_LPTIM_OUTPUT_POLARITY_REGULAR);

        LL_LPTIM_SetUpdateMode(LPTIM2, LL_LPTIM_UPDATE_MODE_IMMEDIATE);

        LL_LPTIM_SetCounterMode(LPTIM2, LL_LPTIM_COUNTER_MODE_EXTERNAL);

        LL_LPTIM_ConfigClock(LPTIM2, LL_LPTIM_CLK_FILTER_NONE, LL_LPTIM_CLK_POLARITY_RISING);

        LL_LPTIM_TrigSw(LPTIM2);

        LL_LPTIM_ConfigTrigger(LPTIM2, LL_LPTIM_TRIG_SOURCE_GPIO, LL_LPTIM_TRIG_FILTER_NONE, LL_LPTIM_TRIG_POLARITY_RISING);

        LL_LPTIM_SetInput1Src(LPTIM2, LL_LPTIM_INPUT1_SRC_GPIO);

        LL_LPTIM_Enable(LPTIM2);

and then:

        LL_LPTIM_StartCounter(LPTIM2, LL_LPTIM_OPERATING_MODE_ONESHOT);

Configuration is based on what STMCubeMX generated. I connected PC0 with function generator 3.3V, 50Hz (signal is valid, checked on osciloscope; for test, later I'll need up to 16kHz, LSE is standard clock quartz 32.768 kHz).

I tried with different configurations, but counter is always 0.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee
Posted on July 14, 2017 at 15:16

Hello

Konieczny.Jakub

,

There is no STM32L487 ! I think you mean 485 or 486 ?

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen