cancel
Showing results for 
Search instead for 
Did you mean: 

Compiler not working

freya17365
Associate III
Posted on May 13, 2016 at 12:56

Hi to all,

I am using Keil and it works fine, but I would like to try STM32F4xx series, so I would like to change compiler.

I tried both EmIDE and CooCox, but I am not able to obatin a working executable.

I realized a working program on Keil (a simple led blinker) and it works.

The same code on the other two compilers doesnt'work.

Here is what I got after compilation:

Keil: Code=976 RO-data=216 RW-data=12 ZI-data=1636

EmIDE: Output size is 8.62 KB

CooCox: Text=1868 Data=1084 BSS=36 Dec=2988

Does someone use EmIDE or CooCox?

How do you configure them?

Is it a GCC problem?

Thank you

Freya

This discussion is locked. Please start a new topic to ask your question.
21 REPLIES 21
freya17365
Associate III
Posted on July 05, 2016 at 19:35

Hi to all,

I got some results. I created another program (a bit more complex) and I compiled it sccessfully. The remaining problem is that all initialization values are lost, so I must write a numeric value or reinitialize variables in runtime.

First question: problem can be ''-fno-common'' option?

I got a sam-ice SWD-usb interface, so, how can I use it for debugging?

I do not know why, ide's do not rcognize it.

Thank you

Freya

________________

Attachments :

Gcc-MisCorrente.7z : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtiA&d=%2Fa%2F0X0000000aW3%2FMB87LIB54qfG4F11zndTTuEzTzuZxMBW79oTvU5RZj8&asPdf=false
Posted on July 05, 2016 at 20:32

The SAM-ICE is locked to ATMEL only devices by the Segger Windows driver.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..