code protection stm32l151cct6
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-05-12 4:22 AM
Posted on May 12, 2017 at 13:22
I'm using a stm32l151cct6 MCU and I want to protect a sector of the flash memory using Option Bytes in ST-LINK Utility.
When I try to use the mode 'write protection', the application code works fine. When I try to use the mode 'read/write protection', it seems that the selected sector memory is erased and the application code don't work.How I can solve the problem please?Thanks.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0