Skip to main content
wlad
Associate
July 19, 2016
Question

cmsis_os.c osPoolAlloc error?

Posted on July 19, 2016 at 14:05

lines in osPoolAlloc function:

index = pool_id->currentIndex + i;

if (index >= pool_id->pool_sz) {

  index = 0;

}

must be replaced with:

index = (pool_id->currentIndex + i) % pool_id->pool_sz;
    This topic has been closed for replies.

    2 replies

    wlad
    wladAuthor
    Associate
    July 20, 2016
    Posted on July 20, 2016 at 10:42

    I've decided to rewrite the whole function :)

    void* osPoolAlloc( osPoolId pool_id )

    {

      if( pool_id == NULL ) return NULL;

      

      uint32_t  pool_sz      = pool_id->pool_sz     ;

      uint32_t  currentIndex = pool_id->currentIndex;

      uint8_t * markers      = pool_id->markers     ;

      void    * result       = NULL                 ;

      int       dummy        = 0                    ;

      

      if (inHandlerMode()) {

        dummy = portSET_INTERRUPT_MASK_FROM_ISR();

      }

      else {

        vPortEnterCritical();

      }

      

      for( uint32_t i = 0; i < pool_sz; i++ ) {

        if( markers[currentIndex] == 0 ) {

          markers[currentIndex] = 1;

          result = (void *)((uint32_t)(pool_id->pool) + (currentIndex * pool_id->item_sz));

          

          currentIndex = (currentIndex + 1) % pool_sz;

          for( ++i; i < pool_sz; i++ ) { 

            if( markers[ currentIndex ] == 0 ) break;

            currentIndex = (currentIndex + 1) % pool_sz;

          }

          pool_id->currentIndex = currentIndex;

          break;

        }

        currentIndex = (currentIndex + 1) % pool_sz;

      }

      

      if (inHandlerMode()) {

        portCLEAR_INTERRUPT_MASK_FROM_ISR(dummy);

      }

      else {

        vPortExitCritical();

      }

      

      return result;

    }

    Richard I
    Visitor II
    February 7, 2018
    Posted on February 07, 2018 at 11:58

    Sorry about reviving an old topic, but the original poster is 100% correct. There is definitely a major bug in osPoolAlloc() in CMSIS_RTOS/cmsis_os.c . The bug is that when the block at index[0] is not marked as free, and the pool was previously full, the pool will fail to allocate other, already freed blocks. Steps to reproduce:

    • Create a memory pool of 10 items
    • Allocate all 10 items
    • Free the last 5 items
    • Try to allocate another item - the allocation will fail
    • Free the first item, then retry allocation, and it will work

    Faulty, original code - note that in the event of index > pool_sz, the index will be stuck at zero for the rest of the loop, if the marker[0] is not free:

    for (i = 0; i < pool_id->pool_sz; i++) {

       index = pool_id->currentIndex + i;

      if (index >= pool_id->pool_sz) {

          index = 0;

      }

       if (pool_id->markers[index] == 0) {

          pool_id->markers[index] = 1;

          p = (void *)((uint32_t)(pool_id->pool) + (index * pool_id->item_sz));

          pool_id->currentIndex = index;

          break;

       }

    }

    Fixed code:

    index = pool_id->currentIndex; // ADDED

    for (i = 0; i < pool_id->pool_sz; i++) {

          // FAULTY LOGIC REMOVED

          index %= pool_id->pool_sz; // ADDED, will wrap index around the bounds

          if (pool_id->markers[index] == 0) {

             pool_id->markers[index] = 1;

             p = (void *)((uint32_t)(pool_id->pool) + (index * pool_id->item_sz));

             pool_id->currentIndex = index;

             break;

          }

          index++; // ADDED

    }

    On another note, it is a bit wasteful to use full bytes to mark occupied blocks. A bitfield would have sufficed and would have required up to 8x less heap.