2012-08-12 6:25 AM
I want to use the HSI, and the code is like the following:
void RCC_Configuration(void) { RCC_DeInit(); RCC_HSICmd(ENABLE); RCC_AdjustHSICalibrationValue(0); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA|RCC_APB2Periph_AFIO|RCC_APB2Periph_USART1,ENABLE); } There is no error during the compilation, but the hardware debug is kind of strange, as shown in the attached. CFGR=0 means that MCO=0, which then indicates that there is no clock at all.... What's wrong ?2012-08-12 11:30 AM
For your unspecified STM32Fxxx part you might need to consider enabling the PWR/BKP clock, and unlocking the BKP domain.
2012-08-12 5:43 PM
Thanks, my part is STM32F107
2012-08-13 6:23 AM
check if the RCC_CR register value is : 0x0000 XX83 where X is undefined.
In default mode, the HSI clock is enabled.2012-08-13 7:38 AM
Sorry, had read LSI/LSE there.
With the HSE/HSI/PLL one has to make sure not to remove the clock from the CPU, and to bring up, and wait for each to be ready before switching over.