cancel
Showing results for 
Search instead for 
Did you mean: 

Change the interrupt frequency

Raül G
Associate II
Posted on April 11, 2018 at 18:08

Hello,

I'm just starting to create a basic code in order to play with the timer interrupt.

Now I have a little problem: my led blinks but I want to change the frequency when I push the button. Why this code inside the main function don't change the frequency?

while

 {

if (!HAL_GPIO_ReadPin(BotoBlau_GPIO_Port, BotoBlau_Pin))      htim14.Init.Period = 10000;

else  htim14.Init.Period = 2000;

 

}

Thanks!

Raul

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on April 11, 2018 at 18:14

Because that's just a variable, and it does not get magiaclly applied to the real physical register of the timer, only when the initialization function is called.

JW

Posted on April 11, 2018 at 21:00

if (!HAL_GPIO_ReadPin(BotoBlau_GPIO_Port, BotoBlau_Pin))      TIM14->ARR = 10000-1;

else  TIM14->ARR = 2000-1;

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..