Question
Change ADC channel
Posted on February 01, 2016 at 09:19
Hello there,
I am using STM32F4. I am trying to use ADC1 to meassure 2 voltages (on channel 8 and channel 7). I want to do it one by one, in polling mode, but I cant figure out how to tell the MCU to change the channel. This is my configuration:/* ADC1 init function */
void MX_ADC1_Init(void)
{
ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION12b;
hadc1.Init.ScanConvMode = DISABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.NbrOfConversion = 2;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.EOCSelection = EOC_SINGLE_CONV;
HAL_ADC_Init(&hadc1);
/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_8;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_7;
sConfig.Rank = 2;
HAL_ADC_ConfigChannel(&hadc1, &sConfig);
}
To measure the voltage I do (test function)
void adc_Init(ADC_HandleTypeDef* handle)
{
assert_param(handle);
p_adc_Handle = handle;
float adcVal = 0;
ADC_ChannelConfTypeDef sConfig;
sConfig.Channel = ADC_CHANNEL_8;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
HAL_ADC_ConfigChannel(p_adc_Handle, &sConfig);
HAL_ADC_Start(p_adc_Handle);
HAL_ADC_PollForConversion(p_adc_Handle, 1);
if ((HAL_ADC_GetState(p_adc_Handle) & HAL_ADC_STATE_EOC_REG) == HAL_ADC_STATE_EOC_REG)
adcVal = adc_GetVoltage(HAL_ADC_GetValue(p_adc_Handle));
sConfig.Channel = ADC_CHANNEL_7;
sConfig.Rank = 2;
HAL_ADC_ConfigChannel(p_adc_Handle, &sConfig);
HAL_ADC_Start(p_adc_Handle);
HAL_ADC_PollForConversion(p_adc_Handle, 1);
if ((HAL_ADC_GetState(p_adc_Handle) & HAL_ADC_STATE_EOC_REG) == HAL_ADC_STATE_EOC_REG)
adcVal = adc_GetVoltage(HAL_ADC_GetValue(p_adc_Handle));
// DODAC pomiar obu kanalow
return;
}
The problem is that after I change to channel 7 from channel 8, I still measure on channel 8. I know that because I measured the 2 voltages with multimeter.
What am I missing here? I would apreciate all help!