2017-05-11 6:25 AM
Hello!
I have CC3100BOOST and STM32F4-Discovery.
I installed IAR, CC3100SDK v 1.2.0, STM32Cube_FW_F4_V1.16.0.
Copied the folder 'Drivers' from '
STM32Cube_FW_F4_V1.16.0.
' to folder 'C:\TI\CC3100SDK_1.2.0\cc3100-sdk\platform\stm32discovery'I opened the project 'C:\TI\CC3100SDK_1.2.0\cc3100-sdk\platform\stm32discovery\example_project_iar\getting_started_with_wlan_station'.
I pressed F7 and there was the error 'Error[Li005]: no definition for 'APBPrescTable' [referenced from C:\TI\CC3100SDK_1.2.0\cc3100-sdk\platform\stm32discovery\example_project_iar\
getting_started_with_wlan_station\Debug\Obj\stm32f4xx_hal_rcc.o]'The developers of Texas Instruments say, that the error is in HAL-driver, and they don't know how to correct the error.
Please, help me!
Thank You!
2017-05-11 6:44 AM
Hi,
I have the same issue with the latest version of cube 4.21. For now I solved it by adding the definition in the file system_stm32f2xx.c
const uint8_t APBPrescTable[8] = {0, 0, 0, 0, 1, 2, 3, 4};
You will have to do it for your processor F4.
2017-05-11 7:03 AM
Giso, thank You for reply!
in file '
system_stm32f4xx.c' there is a string 'const uint8_t APBPrescTable[8] = {0, 0, 0, 0, 1, 2, 3, 4};'
I solved the problem, when I added the string 'const uint8_t APBPrescTable[8] = {0, 0, 0, 0, 1, 2, 3, 4};' in file 'stm32f4xx_hal_rcc.c'.
But I think it is not right(((
Maybe there is another way, not to add
the string '
const uint8_t APBPrescTable[8] = {0, 0, 0, 0, 1, 2, 3, 4};' in file '
stm32f4xx_hal_rcc.c'
?Thank You!
2017-05-12 12:18 AM
I had this problem too. I am using VisualGDB and in my case, when updating BSP to the latest version it caused my project to fail to compile. Reason and fix is as described above. When making a new blank project I could see that this had been added to system_stm32f4xx.c:
const uint8_t APBPrescTable[8] = {0, 0, 0, 0, 1, 2, 3, 4};
So adding it there looks to be the 'correct' way of fixing the issue.
In earlier BSPs, SystemCoreClock, HAL_RCC_GetPCLK1Freq() and HAL_RCC_GetPCLK2Freq() in stm32f4xx_hal_rcc.c all referenced APBAHBPrescTable which was defined in the same file and has since been removed and replaced by APBPrescTable.
For a followup question; Where are these breaking changes documented? I am looking in release notes and cannot find anything about APBAHBPrescTable being removed, or APBPrescTable being added to HAL?
2017-05-12 12:54 AM
Nice to konw that you fixed it.
This issue appeared only in cube 4.21 (for me with lib for F2 V1.60). I totally agree with you something is wrong with the code generation.
2017-05-12 2:10 AM
Hello!
The problem was also solved, when I copied files 'system_stm32f4xx.c' and 'system_stm32f4xx.h' from folder 'C:\TI\
http://www.ti.com/tool/CC3100SDK
_1.2.0\cc3100-sdk\platform\stm32discovery\Drivers\CMSIS\Device\ST\STM32F4xx\Source\Templates' and 'C:\TI\http://www.ti.com/tool/CC3100SDK
_1.2.0\cc3100-sdk\platform\stm32discovery\Drivers\CMSIS\Device\ST\STM32F4xx\Include' to folder 'C:\TI\http://www.ti.com/tool/CC3100SDK
_1.2.0\cc3100-sdk\platform\Stm32discovery'.The file 'stm32f4xx_hal_rcc.c' must be default without adding string .const uint8_t APBPrescTable[8] = {0, 0, 0, 0, 1, 2, 3, 4};
How to create hex or bin file from IAR?
I can't understand(((
Thank You!
2017-05-12 4:39 AM
I solved the problem, thank You!
2017-05-12 6:37 AM
Go in project properties--> output converter and select the format