2018-01-16 02:00 AM
http://www.st.com/en/microcontrollers/stm32l4-series.html?querycriteria=productId=SS1580
'
To simplify migration and give you all the flexibility you need, the STM32L4 is pin-to-pin compatible with the different STM32 series and opens the door to the full STM32 ecosystem.'
2018-01-16 02:53 AM
This docs might be interesting:
'
STM32L4 Series / STM32L4+ Series as well as STM32F405/415 and STM32F407/417 lines
share a high level of
pin
compatibility.Most peripherals share the same
pin
s.The transition from STM32F405/415 and STM32F407/417 lines to STM32L4 Series /
STM32L4+ Series is simple since only a few
pin
s are different.'