cancel
Showing results for 
Search instead for 
Did you mean: 

Can we use a display with 1900x1200 resolution with STM32H743.

Marat Yevtukhov
Associate
Posted on February 21, 2018 at 07:14

We would like to use STM32H743 and 1900x1200 display. From the RM we see that LTDC Active Width Configuration Register (LTDC_AWCR) has 12 bits Accumulated Active Width and 11 bits Accumulated Active Height. That is enough to drive 1900x1200 display. But why datasheet specifies only XGA for the LCD-TFT controller?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Amel NASRI
ST Employee

Posted on February 26, 2018 at 15:05

 Hi yevtukhov.marat‌,

All depends on the characteristics of the LCD display you will be using and mainly its pixel clock.

 XGA isn't really a limitation.

I suggest you refer to https://www.st.com/content/ccc/resource/technical/document/application_note/group0/25/ca/f9/b4/ae/fc/4e/1e/DM00287603/files/DM00287603.pdf/jcr:content/translations/en.DM00287603.pdf (LCD-TFT display controller (LTDC) on STM32 MCUs): even if STM32H7 isn't yet supported in this application note, it can help you to understand more the possible configurations and limitations to interface LTDC with STM32 families.

-Amel

PS: Edited on 27/09/2019 to fix link to AN4861

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on February 26, 2018 at 17:11

Likely to hit a ceiling on the memory bandwidth and refresh rate

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Marat Yevtukhov
Associate
Posted on February 27, 2018 at 06:13

Thank you very much indeed