cancel
Showing results for 
Search instead for 
Did you mean: 

Can the L4R5 OCTOSPI interface be configured as a slave

JButl
Associate

Hi,

Can the L4R5 OCTOSPI interface be configured as an SPI or Hyperbus slave so that it's flash memory can be accessed and addressed via SPI from a master device?

Is it possible to configure the L4R5 OCTOSPI so that the device appears as an external flash memory to an SPI master device?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
S.Ma
Principal

I would think to put this in the STM32 2020 wish list...

The complexity of doing that seems to offer little in the way of rewards.

Perhaps you can make some dual-port mailbox memory with a CPLD/FPGA ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..