cancel
Showing results for 
Search instead for 
Did you mean: 

Can't Recieve/Send data to hc-06

Aozca.3
Associate

my code at below. i can connect succesfull but i cant send any command (like on,off) . what is wrong? help me pls

#include "main.h"
#include "main.h"
#include "stm32f4xx_hal.h"
#include "stm32f4xx_hal_uart.h"
#include "stm32f4xx_hal_usart.h"
#include <stdbool.h> //burda neden uart yok?bilmiyorum unutmus olabilirim yazmayi
 
UART_HandleTypeDef huart2;
UART_HandleTypeDef huart6;
uint8_t deger;
 
char rx6_buffer[50], tx6_buffer[50], rx2_buffer[50], tx2_buffer[50];
bool led_state=false;
int mod_state=0, conf_indeks=0;
void SystemClock_Config(void);
void LED_GPIO_Init(void);
void USART6_Init(void);
 
void clear_buffer()
{	
	for(int i=0;i<50;i++)
	{
		
		rx6_buffer[i] = 0;
		rx2_buffer[i] = 0;
		tx6_buffer[i] = 0;
		tx2_buffer[i] = 0;
				
	}	
}
 
void system_reset()
{
	if(rx6_buffer[0] == 's' || rx2_buffer[0] == 's'){
		
		HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET); // The orange led blinks before the stm board is reset
		HAL_Delay(200);
		HAL_NVIC_SystemReset();
		
	}
}
 
int main(void)
{
  
  HAL_Init();
	USART2_Init();
	USART6_Init(); 
  SystemClock_Config();
  LED_GPIO_Init();
 
	__HAL_UART_DISABLE(&huart2);	
	
  while (1)
  {
		  system_reset(); 
			switch(mod_state){
				
				case 0:			
                HAL_UART_Receive(&huart6, (uint8_t*)rx6_buffer, 50, 500);
		
			          if(rx6_buffer[0] == '1'){	
									
									HAL_UART_Transmit(&huart6, (uint8_t *)tx6_buffer, sprintf(tx6_buffer, "/Conf_Mod"), 500);									
			            mod_state = 1;
			
		            }
					
			          if(rx6_buffer[0] == 'o' && rx6_buffer[1] == 'n'){
			
			            HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_SET);
			            if(led_state != true)
			              HAL_UART_Transmit(&huart6, (uint8_t *)tx6_buffer, sprintf(tx6_buffer, "-->Led is on"), 500);
			            led_state = true;
			
		            }	
		            else if(rx6_buffer[0] == 'o' && rx6_buffer[1] == 'f' && rx6_buffer[2] == 'f'){
			
			            HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_RESET);
			            if(led_state != false)
			              HAL_UART_Transmit(&huart6, (uint8_t *)tx6_buffer, sprintf(tx6_buffer, "-->Led is off"), 500);
			            led_state = false;
		            }								
		   break;
								
			 case 1: 
				       switch(conf_indeks){
								 
								 case 0:								         
                         clear_buffer(); 								 
			                   HAL_UART_Receive(&huart6, (uint8_t*)rx6_buffer, 50, 500);
								 				       			 
		         	           if(rx6_buffer[0] == '0'){	
													 
			                     HAL_UART_Transmit(&huart6, (uint8_t *)tx6_buffer, sprintf(tx6_buffer, "/Normal_Mod"), 500);                          													 
			                     mod_state = 0;
													 
		                     }
												 
							           
							           if(rx6_buffer[0] == 'A' && rx6_buffer[1] == 'T'){
													 
													 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_14|GPIO_PIN_15, GPIO_PIN_RESET);
													 HAL_UART_Transmit(&huart6, (uint8_t *)tx6_buffer, sprintf(tx6_buffer, "#"), 1000); 
													 HAL_Delay(100);
																									 
													 __HAL_UART_DISABLE(&huart6);
                           __HAL_UART_ENABLE(&huart2);
												   conf_indeks = 1;
													  													 
												 }                          											 
								 break;
																
								 case 1: 
									                              							 
												 HAL_Delay(50);												 
			                   HAL_UART_Transmit(&huart2, (uint8_t *)tx2_buffer, sprintf(tx2_buffer, "%s",rx6_buffer), 500);							         	
                         HAL_Delay(50);													 
												 HAL_UART_Receive(&huart2, (uint8_t*)rx2_buffer, 50, 500);
								 
								         if(rx2_buffer[0] == 'O' && rx2_buffer[1] == 'K'){
													 
														__HAL_UART_DISABLE(&huart2);				 
                            HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET); 										    						 
												    __HAL_UART_ENABLE(&huart6);	
								            conf_indeks = 2;		
 
												 } 
                         else if(rx2_buffer[0] == '$') { 
													 											  
													  __HAL_UART_DISABLE(&huart2);
                            HAL_GPIO_WritePin(GPIOD, GPIO_PIN_14, GPIO_PIN_SET); 													 
												    __HAL_UART_ENABLE(&huart6);
													  HAL_Delay(50);												 
			                      HAL_UART_Transmit(&huart6, (uint8_t *)tx6_buffer, sprintf(tx6_buffer, " -->Error, please try again...!"), 500);                        						           												  
													  conf_indeks = 0;	                         
												 }                          	
								 break;
	
								 case 2:
									       HAL_Delay(50);	
									       HAL_UART_Receive(&huart6, (uint8_t*)rx6_buffer, 50, 500);			        
												
                               			 
		         	           if(rx6_buffer[0] == '$'){	
													 	
                           HAL_Delay(50);														 
								           HAL_UART_Transmit(&huart6, (uint8_t *)tx6_buffer, sprintf(tx6_buffer, "%s",rx2_buffer), 500);									
																				          
												   HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET); 													  												 
													 conf_indeks = 0;
													 
											   }					                      											   							         	
                 break;												 
																	
							 }			            			 
			 break;
					    
		  }
  }
}
 
void SystemClock_Config(void)
{
 
  RCC_OscInitTypeDef RCC_OscInitStruct;
  RCC_ClkInitTypeDef RCC_ClkInitStruct;
 
  __HAL_RCC_PWR_CLK_ENABLE();
 
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSICalibrationValue = 16;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
  RCC_OscInitStruct.PLL.PLLM = 8;
  RCC_OscInitStruct.PLL.PLLN = 168;
  RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
  RCC_OscInitStruct.PLL.PLLQ = 4;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    _Error_Handler(__FILE__, __LINE__);
  }
  
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
 
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
  {
    _Error_Handler(__FILE__, __LINE__);
  }
  
  HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
 
  HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
 
  HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
UART_HandleTypeDef UART_InitStruct;
 
 
void USART2_Init(void)
{
 
  huart2.Instance = USART2;
  huart2.Init.BaudRate = 9600;
  huart2.Init.WordLength = UART_WORDLENGTH_8B;
  huart2.Init.StopBits = UART_STOPBITS_1;
  huart2.Init.Parity = UART_PARITY_NONE;
  huart2.Init.Mode = UART_MODE_TX_RX;
  huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart2.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart2) != HAL_OK)
  {
    _Error_Handler(__FILE__, __LINE__);
  }
 
}
 
 
void USART6_Init(void)
{
 
  huart6.Instance = USART6;
  huart6.Init.BaudRate = 9600;
  huart6.Init.WordLength = UART_WORDLENGTH_8B;
  huart6.Init.StopBits = UART_STOPBITS_1;
  huart6.Init.Parity = UART_PARITY_NONE;
  huart6.Init.Mode = UART_MODE_TX_RX;
  huart6.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart6.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart6) != HAL_OK)
  {
    _Error_Handler(__FILE__, __LINE__);
  }
 
}
void LED_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct;
 
  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOA_CLK_ENABLE();
	__HAL_RCC_GPIOD_CLK_ENABLE();
	__HAL_RCC_GPIOC_CLK_ENABLE();
 
  /*GPIO PD12, PD13, PD14 ve PD15 e bagli LED'lerin oncul tanimlamasi*/
  GPIO_InitStruct.Pin 	= GPIO_PIN_12 | GPIO_PIN_13 | GPIO_PIN_14 | GPIO_PIN_15;
  GPIO_InitStruct.Mode 	= GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull 	= GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
}
void _Error_Handler(char *file, int line)
{
  while(1)
  {
  }
}
 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Trying to do 50 bytes and not checking error returns, probably not going to work.

Potential for buffer to overflow when using as a string and not have a trailing NUL.

Not clearing buffers after use.

Try doing it in stages and debug the code

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank yok gör reply. But I am newbie on it. I don’t know how to debug. Please help me. It is important for me. What wrong in my code?