cancel
Showing results for 
Search instead for 
Did you mean: 

Can I disable the STM32 nucleo-32 (L031K6)'s usb commnication port?

DU2
Associate II

hello, I am using L031K6 with UM1956 board.

I am trying ultra low power sensor project with it.

I want to use this board in disabling USB serial communication port status.

because I think it is spending a lot of battery, even though the CPU is in the sleep mode.

Dose it have this option, or possible way to make it?

thank you for read.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
David SIORPAES
ST Employee

You can disable the debugger part altogether by powering the MCU directly from CN4-14 at 3V3. You need to unsolder SB14 and SB9 beforehand. See 6.2.2 paragraph of UM1956 for all available powering schemes details.