2009-04-02 4:33 AM
Can I DeInit only one GPIO-pin Instead of a whole port??? (STM32)
2011-05-17 2:32 AM
Hi all,
I'm relatively new to the STM32 Cortex, and I like to re-init a GPIO Pin. I like to switch between Alternate function and Output open drain mode. But when I use GPIO_DeInit(GPIO_PORT) I reset the whole port instead of only the desired pin. Is it possible to deinit only this pin?? (problem is, an new Init, without the preceeding Deinit it doesn't seem to work) Can anyone help ? Thanks!! RemcoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.