2020-04-20 3:31 AM
Hi,
I am using two STM32F103 Nucleo boards and STM32CubeIDE.
I can see in the oscilloscope the Tx sinal outputs some data when the mode is configured as loopback. But when I switch the mode to normal I can see in the oscilloscope only a short low level pulse and then the channel returns to high level.
Why is this happening?
How can I configure the CAN to work in normal mode?
The first code block is the configuration and the second is the call to transmitt
hcan.Instance = CAN1;
hcan.Init.Prescaler = 16;
hcan.Init.Mode = CAN_MODE_NORMAL;
hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
hcan.Init.TimeSeg1 = CAN_BS1_12TQ;
hcan.Init.TimeSeg2 = CAN_BS2_4TQ;
hcan.Init.TimeTriggeredMode = DISABLE;
hcan.Init.AutoBusOff = DISABLE;
hcan.Init.AutoWakeUp = DISABLE;
hcan.Init.AutoRetransmission = DISABLE;
hcan.Init.ReceiveFifoLocked = DISABLE;
hcan.Init.TransmitFifoPriority = DISABLE;
if (HAL_CAN_Init(&hcan) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN CAN_Init 2 */
TxHeader.StdId = 0x245;
TxHeader.DLC = 1;
TxHeader.ExtId = 0;
TxHeader.IDE = CAN_ID_STD;
TxHeader.RTR = CAN_RTR_DATA;
TxHeader.TransmitGlobalTime = DISABLE;
//filter one (stack light blink)
sFilterConfig.FilterFIFOAssignment=CAN_FILTER_FIFO0; //set fifo assignment
sFilterConfig.FilterIdHigh=0x245<<5; //the ID that the filter looks for (switch this for the other microcontroller)
sFilterConfig.FilterIdLow=0;
sFilterConfig.FilterMaskIdHigh=0;
sFilterConfig.FilterMaskIdLow=0;
sFilterConfig.FilterScale=CAN_FILTERSCALE_32BIT; //set filter scale
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterActivation=ENABLE;
HAL_CAN_ConfigFilter(&hcan, &sFilterConfig); //configure CAN filter
HAL_CAN_Start(&hcan); //start CAN
HAL_CAN_ActivateNotification(&hcan, CAN_IT_RX_FIFO0_MSG_PENDING); //enable interrupts if (HAL_CAN_AddTxMessage(&hcan, &TxHeader, CAN_tx_array, (uint32_t*)&mail_box) != HAL_OK)
{
Error_Handler();
}Thanks!!
Daniel
2020-04-20 5:59 AM
Solved... The CAN Isolator needs 5V and 3.3V but its not showed anywhere.
Also the pin Tx of the board is connected to the Rx of the ADM3053, so fro the ST board is needed to connect the CAN_Tx to the Rx of the CAN Isolator Click (which is connected to the Tx of the ADM3053). :grinning_face_with_sweat: