call to fmount fails in stm32f779I eval board
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-01-03 10:30 PM
Hi STM Community, I am working on one project , for reading a file from sd card and writing it back, And I am using STM32F779I Eval board for it. I am using STM CUBE Mx for generating the code for fatFs and SD card. I am using System workbench for STM32(Ac6) IDE for it. I referred some sample examples. So I made code for like below. But it is always failing at call f_mkfs() goes to error_handler. When I debug into f_mkfs it is failing at disk_write function(
if (disk_write(pdrv, buf, b_vol, 1) != RES_OK) return FR_DISK_ERR; /* Write it to the VBR sector */)
FRESULT res; /* FatFs function common result code */
uint32_t byteswritten, bytesread; /* File write/read counts */ uint8_t wtext[] = 'This is STM32 working with FatFs'; /* File write buffer */ uint8_t rtext[100]; /* File read buffer *//*♯♯-1- Link the micro SD disk I/O driver ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/
if(FATFS_LinkDriver(&SD_Driver, SDPath) == 0) { if(BSP_SD_Init() == MSD_OK) { /*♯♯-2- Register the file system object to the FatFs module ♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/ if(f_mount(&SDFatFs, SDPath, 0) != FR_OK) { /* FatFs Initialization Error */ Error_Handler(); } else {// ♯♯-3- Create a FAT file system (format) on the logical drive ♯♯♯♯♯♯♯♯♯// WARNING: Formatting the uSD card will delete all content on the device if(f_mkfs(SDPath, FM_ANY, 0, workBuffer, sizeof(workBuffer)) != FR_OK) {// FatFs Format Error Error_Handler(); } else { /*♯♯-4- Create and Open a new text file object with write access ♯♯♯♯♯*/ if(f_open(&MyFile, 'STM32.TXT', FA_CREATE_ALWAYS | FA_WRITE) != FR_OK) { /* 'STM32.TXT' file Open for write Error */ Error_Handler(); } #fatfs-sdio #sdcard #f_mount-sdcard- Labels:
-
SDIO-SDMMC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-01-05 2:21 PM
You'll likely need to dig into the diskio.c layer to understand why your write is failing.
Up vote any posts that you find helpful, it shows what's working..